FB#.SCALED.OFFSET

Description

FB#.SCALED.OFFSET sets the offset adjustment for FB#.SCALED.P. It has the same scaling and units as FB#.SCALED.P

Versions

Action Version Notes
Implemented 02-07-01-000

General Information

Type

Read/Write

Units

Same as FB#.SCALED.P

Range

Full position range

Default Value

0.000

Data Type

Float

See Also

FB#.SCALED.P

Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Related Topics

Scaled Feedback